Ecology first for Central Japan Railway Company

Overview_TEXT

Vue d'ensemble

Since its establishment in 1987, the Central Japan Railway Company (JR Central) has vigorously promoted technological development. July 2002 saw the opening of their newest research centre in Komaki in southern Japan.

With a responsible focus on the environment, the new facility incorporates ecological technology in a number of applications, including solar power, cogeneration and ice storage.


The Situation
The 20 hectare complex in Komaki contains over 12,500 square metres of office space, large-scale test equipment, an outdoor test track, a wind tunnel, a Shinkansen Bullet Train driving simulator as well as global environment conservation facilities.

The global environment conservation facilities were to include a 560kW energy-saving cogeneration system. JR Central wished not only to make a contribution to conserving the global environment, but also to be able to pursue technical development in the field of new energy sources.


The Grundfos Solution
Over 50 multistage CR pumps have been installed, playing an important part in the centre’s cogeneration system. In cogeneration, heat energy and electrical or mechanical power is produced from the same fuel in the same facility. Here, waste heat (as in steam) can be used to produce electricity or employed as a heating source.


The Outcome
JR Central presently enjoys low energy consumption, a large amount of free floor space and elegant installation where Grundfos is incorporated into their systems.

Grundfos pumps provide high-quality, reliable operation within hot water circulation, as just one example. The vertical pump category furthermore suits the Japanese market well, where land is sparse.


    Facebook Twitter LinkedIn Technorati

Thème :

Efficient operation - Energy savings - Integrated system solution

Localisation :

Japan

Société :

The Central Japan Railway Company (JR Central)

GRUNDFOS PROVIDED

  • Efficient operation
  • Energy savings
  • Integrated system solution

 

GRUNDFOS PRODUCTS USED

  • 51 CR/CRN pumps

 

CR pumps
Rows of CR pumps shine in Japan performance wise, ecologically and visually.

PRODUCT DATA

The Shinkansen Bullet Train
The Shinkansen Bullet Train makes the 550 km trip between Tokyo and Osaka in approximately 2.5 hours.

TESTIMONIALS
Site designer Takeshi Ushikoshi says: “First of all, the Grundfos CRN multistage pump has an outstanding efficiency and superior running cost parameters. The high efficiency suits our energy saving demands. Moreover, designing the pump installations was facilitated by their in-line design, where we also saved valuable fl oor space.”

 

Site designer Takeshi Ushikoshi
Site designer Takeshi Ushikoshi
Contacts_TEXT

Contact

Si vous avez besoin d'une solution identique, contactez-nous pour de plus amples informations

Téléphone

04 74 82 15 15

Télécopie

04 74 95 58 32

Contact

Si vous avez besoin d'une solution identique, contactez-nous pour de plus amples informations

Téléphone

04 74 82 15 15

Télécopie

04 74 95 58 32